The history of scales dates back to Ancient Egypt, with a simple equal-arm balance on a pivot which compared two masses.
Traditionally, a weighing scale was a device that displayed weight by measuring a deflection, such as a spring scale. In modern weighing machines, scales generally use springs or strain gauge load cells.
How do scales work?
Scales calculate how much something weighs by measuring how much force exists between the object being weighed and the Earth.
Although weighing scales measure force, they can provide measurements of mass in kilograms, grams, pounds as well as other units of measurement. Modern-day scales are more complicated and have a host of uses. Applications range from laboratory weighing of chemicals to weighing of packages for shipping purposes.
From the small fine-tuned laboratory scales to 10 x 120-foot pit-and-girder machines which weigh train cars and tractor-trailers, scales help make modern life possible.
To get a better understanding of how scales operate, it helps to know about mass and weight.
Difference between mass and weight
- Mass is a constant unit of the amount of matter an object has and it stays the same no matter where the measurement is taken. The most common units of measurement for mass are the kilogram (kg) and gram (g).
- Weight is the heaviness of an object. It’s dependent on the gravity on the item multiplied by the mass, which is constant. The weight of an object on the top of a mountain will be less than the weight of the same object at the bottom due to gravity variations. A unit of measurement for weight is the newton (n). A newton takes into account the mass of an object and the relative gravity and gives the total force, which is weight.
Although mass and weight are two different entities, the process of determining both weight and mass is called weighing.
Difference between scales and balances
Weighing scales are similar to balances, however a balance determines mass by balancing an unknown mass against a known mass.
Balances are generally more sophisticated than scales and often used by professionals for advanced scientific weighing in laboratories, universities, medical facilities and research and development related environments. Types of balance include microbalances, analytical balance and precision balances.
It’s commonly accepted that a scale is less sophisticated in precision than a balance, and they’re typically used in food and beverage, health, industrial and commercial industries for weighing ingredients, monitoring personal health and for stocktaking procedures for businesses.
What are industrial weighing scales?
Industrial scales are used for a variety of purposes across many different industries such as agriculture and laboratory.
Industrial scales are designed to achieve the highest accuracy possible and for use in environments which are usually harsher than commercial settings.
They provide essential weighing information for fiscal, legislative and operational purposes. Types of industrial weighing scales range from laboratory scales with capacities of less than 1kg up to large platform floor scales and crane scales with capacities of 10 tonnes or more.